5/9/2020 3:48 PM | |
Posts: 40 Rating: (0) |
I've created my first UDF from a few blocks I already had on my diagram. I see that the resulting function has only one parameter to configure - VMAd. At the same time the individual components have a few parameters each - Float/Int Converter has VM and Res, Analog Amplifier has Point. Is that a limitation of UDF that not all the individual parameters could be exposed in the resulting function? So, if, for example, I need 2 different Point settings, I'll need to create 2 separate UDFs with the individual presets? Attachmentudf_pics.zip (79 Downloads) |
5/9/2020 4:03 PM | |
Joined: 12/18/2014 Last visit: 4/19/2024 Posts: 32847 Rating: (4061)
|
Yes, it looks like you have to create 2 different UDFs. It could be a bug in the software, because it makes no sense that the parameter "Resolution" can be specified as a UDF parameter, but it can't be changed. You should start a Support Request. |
5/9/2020 4:14 PM | |
Posts: 40 Rating: (0) |
Thanks, will try to raise a request. |
Follow us on