9/25/2014 10:28 PM | |
Joined: 12/27/2006 Last visit: 8/18/2024 Posts: 1197 Rating: (113) |
The normal max frekwentie of an input is 4 Hz (See handbook). So i think the minimum time must be 0,25 sec. |
9/25/2014 11:42 PM | |
Posts: 158 Rating: (1) |
ya, that's what I figured, but the timer is looking at the rising edge. Thanks for the reply though. |
9/26/2014 8:38 AM | |
Joined: 12/27/2006 Last visit: 8/18/2024 Posts: 1197 Rating: (113) |
In our world there is a lot of bad elektrical signals. Think on noise and spikes on then net. Wat you want is that the LOGO switchs at goed signals at the input, not on spikes or noise. So every input has an filter, so that quick signals are ignored. Soemens has made the LOGO! for 4 Hz it is 0,25 sec. So every signal at an input that is shorter than 0,25 sec is ignored. But some LOGO! s have an speed input for counters. That input works with max 4 kHz! This input only works on couters, on onthers this inputsignals works like al the others.. What you can do detect a quicer signal than the 0,25 sec: Put the quick input to an counter. That counter counts max to 1 and then you reset this counter The resetpuls of this can you use for the Edge triggerd function. What inpunts are Quick? Its depended of your LOGO! Read the manual. Only avabele on the DC LOGO! The 230V LOGO have Not a quick input.
AttachmentQuick.zip (174 Downloads) |
Last edited by: Toeternietoe at: 9/26/2014 8:56 AMI3, I4, I5, or I6 can by speed inputs, read the manual of your LOGO Programm uploaded |
|
This contribution was helpful to1 thankful Users |
1/23/2017 3:16 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4767 Rating: (123) |
New question published by MMS007 is split to a separate thread with the subject LOGO controller SF command, EDGE TRIGGERED WIPING RELAY. Best regards |
Follow us on