12/16/2014 7:56 AM | |
Posts: 567 Rating: (107) |
Hi Berg, how many cores has your VMware? Maybe that's the reason why you get an error during the installation of the MS SQL Server. Please have look at the following FAQ: http://support.automation.siemens.com/WW/view/en/59703368 Good luck |
This contribution was helpful to1 thankful Users |
12/16/2014 8:26 AM | |
Posts: 32 Rating: (4) |
Hi, here a quote from the PCS 7 Readme V8.1: Installation on computers with multi-core processor When you install the PCS 7 software on PC hardware with multi-core processors in which the number of processors does not equal 2n, or when you use NUMA (Non Uniform Memory Access), you must follow the instructions under entry ID59703368: ● Internet link (http://support.automation.siemens.com/WW/view/en/59703368) PC hardware based on SIMATIC IPC recommended for PCS 7 is not affected by this. Have a look here to find detailed informations about SQL Server 2008 setup issues from the microsoft support site:
|
This contribution was helpful to2 thankful Users |
12/17/2014 1:41 AM | |
Joined: 1/17/2006 Last visit: 8/18/2024 Posts: 553 Rating: (29) |
Hi Ralfinio. I'm only using in VMWare one processor with one core per processor, as shown in the attached file. The problem occurs when installing SQL Server 2008 R2 SP2 - (WinCC). A message is shown about incompability with the file FindSQLinstalls.exe but the installation continues. best regards. |
"Educate the children and it won't be necessary to punish the men." |
|
12/17/2014 1:43 AM | |
Joined: 1/17/2006 Last visit: 8/18/2024 Posts: 553 Rating: (29) |
Have a look here to find detailed informations about SQL Server 2008 setup issues from the microsoft support site: Hi Heisenberg ! Thanks for the material, but I can't install yet. As mentioned, above I'm only using in VMWare one processor with one core per processor, as shown in the attached file. The problem occurs when installing SQL Server 2008 R2 SP2 - (WinCC). A message is shown about incompability with the file FindSQLinstalls.exe but the installation continues. best regards. |
"Educate the children and it won't be necessary to punish the men." |
|
12/17/2014 9:39 AM | |
Posts: 567 Rating: (107) |
Hi Berg, maybe this link from Mirco Soft give a solution: http://support.microsoft.com/kb/969052/en-us Which windows version is used in your VMware? |
12/17/2014 3:14 PM | |
Joined: 1/17/2006 Last visit: 8/18/2024 Posts: 553 Rating: (29) |
Hi Ralfinio. I´m using Windows 7 + SP1 Ultimate 64bit Englishin VmWare Workstation 10. regards. |
"Educate the children and it won't be necessary to punish the men." |
|
4/22/2015 7:18 PM | |
Posts: 21 Rating: (0) |
Dear Berg, I have the same issue. Would you be so kind to publish what was the solution in your case. Thank you. Gabor |
Follow us on