4/22/2016 10:00 AM | |
Joined: 3/14/2008 Last visit: 10/8/2024 Posts: 2109 Rating: (942) |
Did you execute a full compile OS?? |
If I could help you, you can use the RATE button. Thank you. |
|
4/22/2016 10:15 AM | |
Posts: 30 Rating: (1) |
Yes I did but is still the same |
4/22/2016 10:30 AM | |
Joined: 3/14/2008 Last visit: 10/8/2024 Posts: 2109 Rating: (942) |
Hi CKO, The text originates from the text library of WinCC explorer. In my version (PCS7 8.1) it has ID 852 for the text: CiR parameter assignment not successful. There could be something wrong with the text library, which shows the wrong names for the ID number. I had this problem once when I upgraded from v8.0 to v8.1. Suddenly, the text was not showing, but when comparing v8.0 and v8.1 text library, they were different. Here is the topic: https://support.industry.siemens.com/tf/us/en/posts/faceplate-motor-valve-showing-text-error-on-under-command/135522/?page=0&pageSize=10 The entries in the WinCC Text Library are identified uniquely by the "Text-ID" column. During configuration (e.g. message texts in Alarm Logging, names of the message classes and message types, names of the authorization levels) WinCC assigns the text IDs automatically in the text library. There is also an option for editing, deleting and adding texts directly in the Text Library. But, it can also indicate that there is something wrong with hardware configuration. Are you sure the hardware is OK? |
Last edited by: Oreca at: 4/22/2016 10:32:40 AMIf I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to1 thankful Users |
Follow us on