1/19/2017 11:53 AM | |
Joined: 3/14/2008 Last visit: 9/8/2024 Posts: 2094 Rating:
|
Are you talking about CMT (Controle Module Type)? |
If I could help you, you can use the RATE button. Thank you. |
|
1/19/2017 12:22 PM | |
Joined: 1/24/2013 Last visit: 7/19/2022 Posts: 226 Rating:
|
Hi, Yes U are right. CMT - Control Module type CM - Control Module EMT - Equipment Module type EM - Equipment Module |
1/19/2017 1:23 PM | |
Posts: 111 Rating:
|
Hello, you find also more information about this classification based on NAMUR NE33 / ISA S88.1 in following entries: https://support.industry.siemens.com/cs/ww/en/view/78604785 (Specialized for water industry, but also with overall information)
https://support.industry.siemens.com/cs/ww/en/view/53843373 (Specialized for chemical industry, but also with a lot of information / source files) |
Last edited by: nussbaum at: 1/19/2017 1:32:56 PM |
|
1/19/2017 1:27 PM | |
Joined: 2/14/2012 Last visit: 6/18/2024 Posts: 31 Rating:
|
Hello Dinesh KJ, let my try to give you an answer. A block represents a function like channel driver to connect a field device or PID block for controlling a process value. An CM = Control Module is a CFC which contains a different number of blocks, which is necessary for a specific case. An example is a CM for monitoring of an analogue value. Here you have the block to receive the process value using the driver block and one second block for visualization the value in the operator system. An CMT is a type / template which is placed in the master data library and can be copied (instance) in your project. To this topic you can check the application example https://support.industry.siemens.com/cs/ww/en/view/109475748 Equipment Modules are small solutions to a specific automation task like pressure control. Her also one example: https://support.industry.siemens.com/cs/ww/en/view/53843373 Best regard |
This contribution was helpful to
3 thankful Users |
1/20/2017 5:28 AM | |
Joined: 1/24/2013 Last visit: 7/19/2022 Posts: 226 Rating:
|
Hi Star, Good Explanation. -- Thanks Dinesh K |
3/15/2017 10:47 AM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4767 Rating:
|
New question published by K2016 is split to a separate thread with the subject Collect my Control Module Types in folders in the library. Best regards |
Follow us on