5/16/2017 8:12 PM | |
Joined: 9/27/2006 Last visit: 10/17/2024 Posts: 12289 Rating: (2687)
|
Hello nomolina; Documentation for the LMV52 shows a possibilty of Modbus RTU connections; see the screeshot below, taken from the LMV52 product descritption: http://www.scccombustion.com/pdf/LMV52_Specifications_LV5-1020.pdf And the following document shows the Modbus RTU register mapping for the LMV52: https://www.downloads.siemens.com/download-center/Download.aspx?pos=download&fct=getasset&id1=28264 Now: - what experience do you have with Modbus RTU communications? - what CPU are you planning to use for this project (the hardware and software requirements will be different from one CPU family to another)? Please give us the part number of the CPU, and tell us what programming software (and version) you will be using. Let's start with this. More information will be provided when you give us an appreciation of your requirements. Hope this helps, Daniel Chartier |
This contribution was helpful to1 thankful Users |
5/17/2017 7:11 PM | |
Joined: 9/27/2006 Last visit: 10/17/2024 Posts: 12289 Rating: (2687) |
Hello nomolina; Your CPU model is supported by both versions of S7 programming, Step 7 v5.5 (Classic) and Step 7 v13 (TIA Portal). Since you have little experience with S7 programming, you might want to start with the newer software, TIA Portal. Here are links to tutorials provied by Siemens, both as text and video: Siemens tutorials- Step 7 v13(TIA Portal) Look in all the tabs, search for S7-300 sections Video tutorial to get started with STEP 7 (TIA Portal) You will find more video presentation on YouTube, look for the Siemens Channel, search for tIA Portal. Now for the second aspect of this project: what experience do you have with Modbus RTU? On the S7-300 platform you would need to purchase a serial comm. processor CP 341 with a loadable driver (and dongle) for Modbus RTU master. This is quite expensive. Or you could try with this driver proposed by forum member Tibi68, which allows you to use a CP 340 (less expensive) and the driver is at no cost. But support will only come by messaging with Tibi68. MODBUS RTU MASTER FOR CP340/341/441-X (NO DONGLE REQUIRED) A third option exists, using a serial CP 1Si for ET 200S (Profibus slave module), we canlook at it if you need, it results less exensive than the loadable driver but requires a small Profibus-DP network. In all cases, I recommend you start with this presentation by member smiffy, it describes the main pints of Modbus RTU communications, and it has been helpful to start newbies on modbus and as a refresher for programmers with basic understanding of the Modbus protocol. Hope this helps, |
This contribution was helpful to1 thankful Users |
7/4/2017 11:13 AM | |
Posts: 21 Rating: (1) |
USE Serial to porfibus interface SPI3 (RS232 TO Profibus ). Part no 10001236 release 12 make Trebling . network detalil is attached with this msg |
12/4/2017 12:58 PM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating: (172) |
New question published by jgl1359 is split to a separate thread with the subject Interconnect PLC siemens S7 1200 whit The LMV52 Linkageless Burner Management System. Best regards |
Follow us on