5/17/2017 8:48 PM | |
Joined: 2/29/2016 Last visit: 3/12/2024 Posts: 100 Rating: (1) |
Very helpful Oreca, I've been struggling with this for quite some time also..I also have a problem with Eventstate...When using group display, I cannot see alarms, also I cannot lock/unlock messages. I see a very weird value for Eventstate something like 132130342, a very long number. I'm using two MsgEvId1 and 2, where 2 is a spare for later use. What can be the problem....grrr ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 5/18/2017 10:37:08 AMNew subject after splitting |
|
6/20/2017 7:59 AM | |
Joined: 3/14/2008 Last visit: 9/27/2024 Posts: 2098 Rating: (938)
|
Hi DaytonaM, Are you using MsgEvID2 in your code? Because I had a problem once where I just declared MsgEvID2 (VAR_INPUT), but did not use this in my code (just for spare). But, then I could not lock/unlock messages in the faceplate. After removing the variable, AS+OS compile/download suddenly it worked. |
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on