12/22/2017 9:08 AM | |
Joined: 5/16/2014 Last visit: 9/12/2022 Posts: 7298 Rating: (2164)
|
Hello vorapob, the internal variable "@CurrentUser" is a systemvariable and will be created automatically, when you create a new project. It contains in Runtime the name of a user, which has logged in successfully. The users, and their authorization-levels can you create in the User-Administrator of WinCC. Regards Georg Berghof |
PS: If this post did really help you, you may use the Rate-button |
|
12/22/2017 9:30 AM | |
Joined: 1/17/2013 Last visit: 9/3/2024 Posts: 1103 Rating: (6) |
Dear Experts, What is the meaning of NO. 1000 ? Is it a user authorize level ? Best Regards, Vorapob |
Best Regards, |
|
12/22/2017 10:51 AM | |
Joined: 5/16/2014 Last visit: 9/12/2022 Posts: 7298 Rating: (2164)
|
Hello vorapob, the Authorization-Levels "1000", "1001" and "1002" are special systemlevels for using with Client-PC without own projects ("1000" and "1001") or for Web-Clients/DataMonitorClient (1002). Regards Georg Berghof |
PS: If this post did really help you, you may use the Rate-button |
|
12/25/2017 4:15 AM | |
Joined: 1/17/2013 Last visit: 9/3/2024 Posts: 1103 Rating: (6) |
Dear Export, I wonder about .OCX file. How can I create new one of .OCX file ? How can I edit from source file as attached files ? Thank you very much. Vorapob |
Last edited by: vorapob at: 12/25/2017 4:16:04 AMBest Regards, |
|
This contribution was helpful to1 thankful Users |
12/25/2017 4:16 AM | |
Joined: 1/17/2013 Last visit: 9/3/2024 Posts: 1103 Rating: (6) |
|
Best Regards, |
|
Follow us on