5/17/2008 7:23 PM | |||
Posts: 5822 Rating: (412)
|
Hello, well, I would personally say you have two chances. The first one is OPC, no doubt. I guess using the Toolbox with a SIMATIC NET OPC Server is the way is the most promising one. The second way I found in the Forum, at
There seems to be a DDE Server but only for SINUMERIK, I guess. Check it out if you want. Best regards J_Bell |
||
5/19/2008 4:57 PM | |
Posts: 5822 Rating: (412)
|
Hello candyengineer, I am looking forward to hear from your solution. Situations like that are always very exciting. Best regards J_Bell |
5/23/2008 6:10 PM | |
Joined: 10/31/2005 Last visit: 9/4/2024 Posts: 366 Rating: (31) |
candyengineer, it would be really nice if you inform about the result. Cheers! |
6/3/2008 1:52 PM | |
Posts: 1 Rating: (0) |
Dear candyengineer, You can use the product "PLC Link for SIMATIC STEP7" from HybridTech (www.plclink.com) to transfer Simulink block diagrams and Stateflow charts to SCL code directly runable under SIMATIC. Interface to Simulink is performed via OPC connectivity. You can download a demo version from the website. Best regards Lasse Ibsen |
7/14/2017 12:31 PM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating: (172) |
New question published by ValTargaryen is split to a separate thread with the subject Is it possible to connect LOGO 8! with MATLAB?. Best regards |
Follow us on