2/15/2018 1:38 PM | |
Posts: 6 Rating: (0) |
Good morning, I am searching for some parameters on the expert list of the micromaster440 . but these parameters are fro level 4. And on the manual it says that these parameters are not visible with BOP or AOP thank you ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 2/16/2018 10:56:00 AMNew subject after splitting |
|
2/15/2018 2:37 PM | |
Posts: 531 Rating: (34) |
Isn't starter the software which is free and can be used with MM4? |
Follow us on