2/4/2020 8:55 PM | |
Joined: 9/27/2006 Last visit: 10/17/2024 Posts: 12289 Rating: (2687) |
Hello t4yy4b; Siemens has often used HMS as a third-party provider of CANopen equipment. For the S7-1200, they have developed the CM CANopen, as seen in the following Application Example: https://support.industry.siemens.com/cs/us/en/view/109479771 From the entry for the CM CANopen in the Siemens Industry Mall, read this very important notice : NoteThe CM CANopen module is an HMS Industrial Networks product and can only be obtained through HMS. Please note that ordering and support for the module are exclusively carried out via HMS Industrial Networks. Please contact HMS Industrial Networks directly should you have any questions concerning this module. The relevant contact details can be found on the Internet at http://www.ixxat.com/cm-canopen Further information can be found in these webpages: http://www.ixxat.com/products/products-industrial/plc-extensions/cm-canopen http://www.ixxat.com/support/file-and-documents-download/demos Hope this helps, Daniel Chartier |
This contribution was helpful to1 thankful Users |
2/18/2020 5:25 PM | |
Joined: 1/15/2020 Last visit: 2/18/2020 Posts: 6 Rating: (0) |
Thanks for the responses guys! I will most likely have a look at the CM CANopen module from HMS |
Follow us on