5/12/2021 11:32 AM | |
Posts: 9 Rating:
|
I'm sorry I meant to say DC to DC step down from 24vdc to 12vdc. Here is the link to what I have 24VDC to 12VDC, I also have one for 12vdc to 5vdc. I just finished making a small trainer kit for the LOGO that will later upgrade to the s7. Everything works in LSC, I can see the values change. I do not have a specific program to display on the HMI, I just wanted to test out the analog pots from LSC to TIA. Even if the program on LSC is just an analog input. I want to display to output of the pot through a level indicator or just value on a I/O label on the HMI. The version of TIA is 16.0, but the HMI is running on 15.1 because I have to update the image for the HMI that I have apparently. I havn't did that yet, but everything works on the HMI. I've tried all the digital and output to display perfectly on the HMI except for the analog. |
Last edited by: David119 at: 05/12/2021 11:34:22 |
|
Follow us on