10/11/2011 11:12 AM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181)
|
In order to configure a connection between IFix and S7 PLC one example - Connecting IFIX SCADA to Siemens S7 using TCP/IP So, in your case you will have two connection (to each CP). Basically they will be the same, the only differences will be IP addresses. In IFix you can make a watchdog in order to trace each connection. And in case of fault (connection 1), IFix to start reading from connection 2 and vice verse. I am sorry don't know if this scenario is possible for sure in IFix and specially how to realize it under IFix... Best regards, Hristo Mihalev |
5/17/2017 12:35 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4772 Rating: (123) |
New question published by Esam is split to a separate thread with the subject Connect Siemens H station with kepware opc server. Best regards |
Follow us on