8/11/2012 11:09 AM | |
Posts: 1064 Rating: (72) |
it should be on if24 v dc is applied to the processor. it tells you the internal 5 v power supply is ok |
8/12/2012 9:42 AM | |
Joined: 6/12/2009 Last visit: 4/27/2024 Posts: 20 Rating: (0) |
Thank you |
8/12/2012 9:44 AM | |
Joined: 6/12/2009 Last visit: 4/27/2024 Posts: 20 Rating: (0) |
This means 5VDC LED should be on always after power On. |
8/13/2012 7:56 AM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181) |
|
Follow us on