8/9/2019 4:11 PM | |
Joined: 4/28/2015 Last visit: 2/29/2024 Posts: 8 Rating: (1) |
Hi everybody Passing here to share my experience with ALFA 3101C with ethernet port, this is a very popular weight indicator here in Brazil. The Alfa 3101C use an Wiznet (wiz750r) serial to ethernet converter. You need to configure the device using the respective manual, set ip adress and communication port, I used por 502 and set the device to master mode, so, with this the device send conituously the NTWeight and Tara values using ASCII format. On PLC side the connection was made using the TCON block, and the data received with TRCV block. On document attached its possible to show some details. Br. Attachmentread data from ALFA 3101C using TCON and TRCV Siemens.pdf (42 Downloads) |
Follow us on