11/19/2014 5:16 PM | |
Posts: 22 Rating: (0) |
Hey Friends, Ive got a big problem, i dont know how to declare properly an input from Logo in the Visualisation(HMI) to be able to can control it also from the HMI. I want to can give also values in the panel and this values to be sent at the LOGO! analog input. Which would be the Shortname for an analog input from Logo in HMI ? I add also a picture. This is my actual status, in which i can see the value from this analog input but i cant give any value in that field. Thank you in advance! Regards, Klaus AttachmentAnalogeingang.pdf (514 Downloads) |
11/20/2014 11:10 AM | |||||||||
Joined: 2/8/2012 Last visit: 12/22/2014 Posts: 2347 Rating: (385) |
Why do you ask your questions both in the German and English speaking forum in? The analog flag 1 has variable memory (VM) Address VW1118. And this address is then also in the visualization. |
||||||||
Follow us on