1/16/2014 3:07 PM | |
Posts: 13 Rating: (0) |
Hi Is it somehow possible to change the value "On threshold" in an "Up/down counter" via an analog input (0-10V)?
|
1/18/2014 8:29 PM | |
Joined: 12/27/2006 Last visit: 8/18/2024 Posts: 1197 Rating: (113) |
Yes thats possible, only if you use a LOGO 0BA6 or 0BA7 Look in the attachment And.. You can use Di7 as Analog input and Di8 as digital input. Even, if you can programm, u can use a single inpu zb Di 7 as a analog inout and as a digtal input. Then you have to make a sort of multiplexing Look in the attachment In the second part of the sceme ther is a kind of multiplexing AttachmentAnalog_tresholt.zip (219 Downloads) |
2/4/2014 8:04 AM | |
Posts: 340 Rating: (6) |
new question is splittet to isn't it possible to use only one of the LOGO! V6 digital inputs as an analog input? |
Follow us on