1/22/2021 8:01 PM | |
Joined: 12/18/2014 Last visit: 9/22/2024 Posts: 33813 Rating: (4201)
|
Which LOGO! do you have exactly? Can you make and upload a screenshot of your login screen?
|
1/22/2021 9:30 PM | |
Joined: 12/18/2014 Last visit: 9/22/2024 Posts: 33813 Rating: (4201)
|
Please can you upload your LWE project and your LOGO! program as a ZIP file? |
1/23/2021 1:42 PM | |
Posts: 7 Rating: (0) |
Good morning I have attached the file to this post. Thanks a lot. AttachmentProyecto ISAGEN 2.zip (153 Downloads) |
1/23/2021 1:45 PM | |
Joined: 12/18/2014 Last visit: 9/22/2024 Posts: 33813 Rating: (4201)
|
It's only the LWE project. Where is the LOGO! program? |
1/23/2021 3:42 PM | |
Posts: 7 Rating: (0) |
Sorry, Here's the program...
AttachmentISAGEN cerramientos.zip (157 Downloads) |
1/23/2021 5:27 PM | |
Joined: 12/18/2014 Last visit: 9/22/2024 Posts: 33813 Rating: (4201)
|
I guess there is a problem with the LWE project. I cannot save it to the SD card via LWE if the SD card is in the LOGO!. If I plug the SD card into the PC and then I transfer the project to the SD card, this works. If I then insert the SD card into the LOGO! and call up the extended web server, the pages are displayed to me. The images are also animated and the 4 buttons (M11, M12, M18 and M19) also work. However, I have the current LWE V1.1.0. In order to be able to work with your old LWE project, I had to upgrade it.
AttachmentIsagen.zip (140 Downloads) |
Follow us on