3/10/2016 6:23 PM | |
Posts: 65 Rating: (1) |
Attached is cut down version of the issue I am sometimes seeing. I use counters to store display time (6 seconds in this case) and input hold time (5 seconds) as they are used in many places in my designs. You can see the connection B272 to B021 (and associated counter value in B021) but there is no visible connection between B273 and B259 even though the counter value, 500, is set correctly. Makes it rather hard to edit the connection... In the full design, this missing connection goes to many places all the same, counter value correct, but no sign of visible connection. AttachmentMissing Connection.zip (101 Downloads) |
3/21/2016 5:47 PM | |
Posts: 65 Rating: (1) |
Attached is another .lsc file that causes a NullPointerException in Soft Comfort 8. Load the file into Soft Comfort and expand the parameter boxes. Upon expanding the 2nd one you will get a Java Exception error. Bit annoying as it now fails to show the connection. Also sometimes forgets the "unit", in that Off delay was set in seconds but file open with Off delay defaulting to milliseconds. AttachmentMissing Connection 2.zip (91 Downloads) |
Follow us on