1/25/2015 1:01 PM | |
Posts: 21 Rating: (0) |
PLS reply me |
1/25/2015 1:01 PM | |
Posts: 21 Rating: (0) |
PLS help me |
1/25/2015 6:55 PM | |
Joined: 1/17/2010 Last visit: 8/21/2024 Posts: 77 Rating: (5) |
Try to delete the project and create it agian. |
1/26/2015 9:09 AM | |
Posts: 567 Rating: (107) |
Hi, there are a lot of reason why a OS download isn't possible. Please check the points of the following FAQ: http://support.automation.siemens.com/WW/view/en/33123686 |
1/26/2015 1:44 PM | |
Posts: 21 Rating: (0) |
I tried to download this OS project by changing the path & I already checked access rights its ok but still I m facing same error. |
1/26/2015 1:52 PM | |
Posts: 567 Rating: (107) |
Hi, check your network settings: - correct network adapter selected in SIMATIC Shel (for terminal bus) - network adapter for terminal bus at the first place in the advanced network settings of windows - ... For more information have look at the PCS 7 compendium part A: http://support.automation.siemens.com/WW/view/en/107196780 Maybe you download the OS project by using the plant bus. In this case the download of the project (the files) is possible but to open the project remote not. |
1/26/2015 1:56 PM | |
Posts: 21 Rating: (0) |
I m facing this error while downloading to the target project not after not at the time of opening. Here is the snapshot of error message. |
Follow us on