3/4/2018 7:40 PM | |
Posts: 200 Rating: (6) |
Hi All I am continuing my learning of programming and have a couple of question regarding a part of a program that i am working with (see attached file) i want to make sure that my scaling of the input is correct when displaying the levels and in relation of the water in the tank. So to the bottom of the level sensor its 2m and to the overflow of the tank its 1.8m and then with the switching points in the middle. So how do i confirm that this is where i am correct with scaling also how would i change it from the meters of water in the tank to the liters used if the tank is holding 9000 liters Thanks Andrew AttachmentFill_level_V3.zip (99 Downloads) |
3/4/2018 8:02 PM | |
Posts: 200 Rating: (6) |
Hi so in my bar graph i have changed the 2.3m to 2m and the scaling from 205 to 200 B001 am i correct |
This contribution was helpful to1 thankful Users |
3/4/2018 8:21 PM | |
Joined: 12/18/2014 Last visit: 9/20/2024 Posts: 33801 Rating: (4199)
|
Here version 4 with liters.
AttachmentFill_level_V4.zip (120 Downloads) |
This contribution was helpful to2 thankful Users |
3/7/2018 11:17 PM | |
Posts: 200 Rating: (6) |
Hi This is great i have had a go on my bench setup and works a treat Thanks for the Help |
This contribution was helpful to1 thankful Users |
3/8/2018 7:44 AM | |
Posts: 42 Rating: (5) |
nice @ixo65.
|
Follow us on