5/16/2014 11:29 AM | |
Joined: 4/19/2008 Last visit: 1/12/2021 Posts: 1525 Rating:
|
Hello kijo, Which Cable you have ? For establishing connection between S7 200 PLC and PC via USB interface, you have two possibilities. 1. 6ES7901-3DB30-0XA0 2. 6ES7972-0CB20-0XA0This cable is more expensive than the previous one because you can use it to communicate to S7 200 and S7 300 / S7 400 as well. Also Have a look on the How can I select USB-PLC Data Cable |
Ammy |
|
5/16/2014 2:14 PM | |
Joined: 2/18/2014 Last visit: 9/23/2020 Posts: 79 Rating:
|
And there is no other way to transfer the program from PLC to PC except with this cable? |
5/16/2014 2:50 PM | |
Joined: 5/28/2008 Last visit: 2/25/2021 Posts: 4205 Rating:
|
Hello together, Although the above words are mine as per my post in the above mentioned thread but it was an old post from 2010. Just an update here is the PC adapter with part number "6ES7972-0CB20-0XA0" is a phased out product as from Nov. 2013. You have to oder the new one "6GK1571-0BA00-0AA0"
For all possibilities to Connect (Upload and download to S7-200)
And please note the followings:
Hope this helps. |
Ayman Elotaify |
|
This contribution was helpful to
2 thankful Users |
Follow us on