6/16/2010 10:08 AM | |
Joined: 4/8/2010 Last visit: 12/12/2011 Posts: 31 Rating: (0) |
thank you for the quick answer! |
6/16/2010 10:53 AM | |
Posts: 661 Rating: (123) |
Hi kostas, is networking really necessary? What kind of data do you want to transfer between the devices? I know applications like yours, but normally it´s enough to have a pushbutton locally for each blind (up/down). Additionally, if you want to have a central control to let all blinds (in all floors) move up or down, wire central control pushbuttons and connect them in parallel to all 4 LOGO! devices. An example you can find here: Control for 8 shutters with central control for UP/DOWN |
6/17/2010 9:12 AM | |
Posts: 153 Rating: (16) |
To connect 4 or 5 devices it is possible. But it is required to know precisely what signals should accept and transfer each device. For transfer and reception it is required to use inputs and exits. At use instabus the big flexibility in data transmission possibility between devices is reached. In my opinion instabus this decision for fast input in operation of all system.It is required: CM EIB/KNX the module for everyone LOGO! (Power supply 24 V AC/DC) , Cable for a network KNX, power supply - SIEMENS N 125 KNX/USB - SIEMENS N 148/11 Software ETS3 and LOGO!SoftComfort
AttachmentLOGO!_EIB_e.pdf (619 Downloads) |
Follow us on