12/2/2020 1:59 PM | |
Posts: 1 Rating: (0) |
Hello, I need to control a hydraulic valve in LWE with use push button. The solution from above is working (the signal are change at the falling edge) but I need a continouslu signal when the push button is presset and no action when the button is no pressed. So as long as the button is pressed in need a signal. Thank You in advance ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 12/03/2020 07:48:49New subject after splitting |
|