7/17/2008 8:32 PM | |
Joined: 1/5/2007 Last visit: 4/7/2023 Posts: 1690 Rating: (580)
|
Hi FDRG, the LOGO! typ 0BA5 (and older series) it is not possible to put more than one actual value (of a block) at one textbox line! The handbook of the new comming series 0BA6 contains no infos how many actual block values can be set into one textbox line (one line can have 24 characters). To put two smal actual values into one line at a textbox it gives a trick. Look at the attachment. You find an example of an own counter for time in hourers am minutes (of a signal).The second page of the sheed contains a circuit round a comparator, witch is used to build one value with a decimal point from two smal (0..327 and 0..99) integer values and show this "decimal" value at a textbox (--> "0.0" ... "327.99". The "decimal" point is now the separator of the two integer values... I hope this can help you? Best regards Betel AttachmentTest_Betriebsstundenzähler_V1.zip (783 Downloads) |
==> Meine TAG-Listen: "deut." |
|
7/24/2008 9:03 PM | |
Joined: 1/5/2007 Last visit: 4/7/2023 Posts: 1690 Rating: (580)
|
Hi FDAG, |
==> Meine TAG-Listen: "deut." |
|
Follow us on