10/14/2019 9:08 AM | |
Joined: 5/3/2017 Last visit: 4/19/2024 Posts: 673 Rating: (216) |
Hello Dmitry Anyushin, you can't use CPUs with different firmware as H-System. For a H-System you have to use the identical CPUs (thats include the firmware). See the manual SIMATIC Fault-tolerant systems S7-400H at section 3.2 Rules for the assembly of fault-tolerant stations. So you have to update the firmware of the old controller. With regards |
This contribution was helpful to2 thankful Users |
10/14/2019 9:17 AM | |
Joined: 2/9/2012 Last visit: 8/15/2022 Posts: 32 Rating: (0) |
Thank you very much! |
Follow us on