7/11/2019 7:23 AM | |
Posts: 3 Rating: (0) |
Dear colleges! I need your opinion about DOR 560L-6-159 motor. In attachment you can see file with characteristics of installed and new motors. They have some differences in characteristics. These motors are using in conveyor belt systems. 4 motors in one drive station. Controlling system is Simovert Master Drive. Пусковой момент (MA/MN) / Starting-/ Rated torque (TS/TN)1.1 0.9 Максимальный момент (MK/MN) / Breakdown-/ Rated torque (Tmax/TN)2.9 2.0 These chracteristics, different values are critical? If possible, I need your quick replies AttachmentКопия Сравнительная таблица Двигателя DOR 560.xlsx (109 Downloads) |
7/12/2019 6:34 AM | |
Posts: 3 Rating: (0) |
One motor connected to one frequency converter. System mster-slave. Four motor works on the drive station. |
Follow us on