7/20/2008 11:16 AM | |
Posts: 2 Rating:
|
Hi All, I am looking for a double tap button configuration. I want to be able to push button I1 once and the Q1 should be on. I want also to tap I1 twice and Q2 should be on without Q1 flashing. I did some testing, maybe you can start from the attached file. The first drawing is the kind I wanted, the second is the tapping twice function alone. Thanks for helping in advance. Attachmentdouble tap button.zip (321 Downloads) |
7/21/2008 8:39 PM | |
Joined: 1/5/2007 Last visit: 1/10/2021 Posts: 1685 Rating:
|
Hello liekyfreakie,
Betel AttachmentDEMO_single_and_double_tab_detection.zip (1543 Downloads) |
==> Meine TAG-Listen: "deut." |
|
This contribution was helpful to
1 thankful Users |
7/23/2008 9:59 PM | |
Posts: 2 Rating:
|
Hey, thanks man. Works fine. This reduces the amount of inputs. |
7/24/2008 9:04 PM | |
Joined: 1/5/2007 Last visit: 1/10/2021 Posts: 1685 Rating:
|
Hi liekyfreakie, |
==> Meine TAG-Listen: "deut." |
|
10/8/2009 12:00 AM | |
Posts: 1 Rating:
|
Thnx guys, i was struggling on the same issue, now i understand how to feed back certain states of timers (recursions can only be done by....) At last i get this.. MARKERS.... ThnX a lot, i changed the program a little bit so i push short or long to activate different outputs...
AttachmentLang-kort-drukken.lsc.zip (201 Downloads) |
Last edited by: Herzwam at: 10/8/2009 12:02 AM |
|
10/9/2009 9:33 AM | |
Joined: 1/20/2006 Last visit: 8/16/2018 Posts: 661 Rating:
|
Another way to do this is shown here: http://www.automation.siemens.com/logo/html_76/products/02Applications/index.html called : "Controlling 2 outputs with 1 button" |
10/9/2009 3:41 PM | |
Joined: 1/5/2007 Last visit: 1/10/2021 Posts: 1685 Rating:
|
Hi FUX, hi SIEMENS support team, sorry, but the shown circuit is not a filter it is only a memory - needs more LOGO!-memory as the combination of multiplexer + amplifiver but value can be memoried retentive! But the circut give only give a random value at variable measuring time to the circuit - that is not a filter it is only a slower rate of value actualisation !!! Best regards Betel |
==> Meine TAG-Listen: "deut." |
|
Follow us on