10/22/2019 6:44 AM | |
Joined: 5/12/2006 Last visit: 4/26/2024 Posts: 22231 Rating: (2980)
|
hello, no without memory card a FW change is not possible. regards christoph |
10/22/2019 8:06 AM | |
Joined: 5/12/2006 Last visit: 4/26/2024 Posts: 22231 Rating: (2980)
|
hi, i think he mean 4.7 SP10 down to V4.7 without SP. It can be that he have not the 4.7 SP10 SSP installed and can not select the version 4.7 SP10 in the HW Catalog. The SSP for V4.7 SP10 for starter can be downloaded here: https://support.industry.siemens.com/cs/ww/en/view/109757079 Regards Christoph |
This contribution was helpful to1 thankful Users |
10/22/2019 3:14 PM | |
Joined: 3/9/2016 Last visit: 4/11/2023 Posts: 35 Rating: (0) |
In this document it says it cannot support SD cards bigger than 2 GB
AttachmentConverter with the CU240B-2 and CU240E-2 Control Units (002).pdf (64 Downloads) |
10/22/2019 4:14 PM | |
Joined: 3/9/2016 Last visit: 4/11/2023 Posts: 35 Rating: (0) |
Hey Chris, you're a life (job) saver lol Thank you for the help. :) |
Follow us on