7/29/2019 11:13 AM | |
Joined: 8/3/2009 Last visit: 4/23/2024 Posts: 12834 Rating: (1639) |
Hello Perhaps this one contains some information for you: https://support.industry.siemens.com/cs/de/en/view/21848242 Bye Murof |
If this Information really helps, you could use the Rate function |
|
8/19/2019 10:00 AM | |
Joined: 3/26/2018 Last visit: 11/8/2023 Posts: 38 Rating: (1) |
Hi Murof,
So I Still don't have an answer. I Think I need to use the HW_ID which is an INT, but if I put this variable on the LADDR from DPRD_DAT and it gives an error: Data type 'Int' cannot be converted implicitly into data type HW_IO' -> I think it is the DPhead (or is it the slave?) I just want to read data out of an Profibus connection and write it to a DB which is declared by an input. so If I put 5 in the input: Read data and write this to DB#5 Does somebody know how to do this? Best regards, |
Follow us on