8/21/2019 10:25 PM | |
Joined: 1/15/2019 Last visit: 10/27/2021 Posts: 16 Rating: (0) |
Hi guys, Quite a similar case. I`d like to establish link between CPU 1511-1 and 3rd party SCADA over IEC 60870-5-104 and IEC 61850 protocol. If the SCADA is TCP/IP visible and supports IEC 60870-5-104 protocol, do I still need to use TIM 1531 IRC communication module as a gateway or is it enough to use SIRPLUS RIC library on CPU? I`d like to avoid using TIM as it costs fortune. Thanks a lot for any useful information. Regards, Banchy ------------------------------------------------------------------------------------------ |
Last edited by: banci at: 08/21/2019 22:52:20Last edited by: Jen_Moderator at: 08/22/2019 11:18:19New subject after splitting |
|
Follow us on