9/9/2019 12:17 PM | |
Joined: 3/27/2008 Last visit: 4/17/2024 Posts: 1090 Rating: (137) |
https://support.industry.siemens.com/cs/ww/en/view/12745006 A braking resistor may provide a short term fix, but it will not be correct, because the resistor will be wasting a considerable amount of energy, and over time the capacity of the resistor may be exceeded. The above link is a 'look at' the Droop Control, and is the correct solution for these applications, typical for multiple motors connected to the same mechanical load, long line conveyors, chain conveyors, and some aggregate conveyor systems. This Droop Control, can be configured without any extra 'kit', and is effective.
|
Last edited by: Jen_Moderator at: 09/09/2019 12:29:21Optimized link. Tractor |
|
9/11/2019 3:25 AM | |
Joined: 1/5/2016 Last visit: 2/27/2024 Posts: 49 Rating: (1) |
exactly my application is chain conveyors. and im having problem with synchronizing speed. speed motor is not same during overtime then the slower motor going to generating mode. thank you for help. let me try your sulotion. i never do that before. |
This contribution was helpful to1 thankful Users |
Follow us on