5/27/2019 6:28 AM | |
Joined: 2/20/2014 Last visit: 4/23/2024 Posts: 395 Rating: (38) |
Hi, I am getting error 16#80C8 at the master block. Please advise on what could cause this. I have attached the sample program here. ------------------------------------------------------------------------------------------ Attachment47756141_Sample_project_for_STEP_7_TIA_Portal_V15.zip (186 Downloads) |
Last edited by: Jen_Moderator at: 05/27/2019 08:28:26New subject after splitting |
|
6/11/2019 11:23 AM | |
Joined: 2/20/2014 Last visit: 4/23/2024 Posts: 395 Rating: (38) |
Hi, Attached is the photo of the VSD that is being used now & the wiring (RS 485) therefore using mode "0". Besides, termination resistor also was used on both ends (120 ohm resistor at the VSD end & 220ohm ohm resistor at PLC COM module). Also tried with another cable (without resistor on both ends (but still getting error 16#80C8). Already check the baud rate, parity but still getting the same error code. How can overcome this? AttachmentForum upload Modbus_2019JUNE11.zip (196 Downloads) |
Follow us on