10/19/2014 9:26 PM | |
Joined: 3/14/2008 Last visit: 5/7/2024 Posts: 2066 Rating: (928) |
Yeah, there is. Go to the block and check which fb is allocated to the block. In blocks folder, find the fb and open it. In the top you can select all i/o that is available to the block. Find the i/o that you want to change and right mouse click on it. You can enter a menu whereyou can type in block attributes such as s7_unit, s7m_c etc... then after the attribute, give in the value true or false and click ok. Save the block. Now when you enter cfc, you notice the block attributes are changed for all the blocks of the block type you modified
|
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on