9/15/2014 6:01 AM | |
Joined: 1/21/2013 Last visit: 9/4/2024 Posts: 4620 Rating: (707) |
Hello Nicki, Watch the video to get an idea of how to get into programming, and you have to find the function RS if you want to do it with two inputs, depends on the version that you have, if you have 0BA0 you only have RS, if you have 0BA1 and more you can do it even with a single input (download the software that you can understand better) if you have a computer on the hand download the trial version of LOGO! It's free How to program siemens logo - YouTube LOGO! Demo software , upgrades/updates, drivers ... - Siemens Watch the latest numbers of the code and you will have your version: example 6ED1 052-1MD00-0BAx the number that is in the place of x means your version 0.1.2.3.4.5.6.7 I tell you this because the version that you have the functions are more, if you have the high number To choose the version, start the software open new project and press CTRL + H |
Last edited by: Ste39 at: 9/15/2014 6:34 AMLast edited by: Ste39 at: 9/15/2014 6:33 AMLast edited by: Ste39 at: 9/15/2014 6:14 AM |
|
9/15/2014 8:48 PM | |
Joined: 2/8/2012 Last visit: 12/22/2014 Posts: 2347 Rating: (385) |
Hello, you want a two-way circuit? |
9/15/2014 9:04 PM | |
Posts: 9 Rating: (0) |
I think that's what it is. I want to control the same output from 2 different inputs. Do I need to wire it, or can it be done with the plc itself. If yes, how? |
9/15/2014 9:10 PM | |
Joined: 2/8/2012 Last visit: 12/22/2014 Posts: 2347 Rating: (385) |
Ifboth switches pulsedor continuous signal? |
9/15/2014 9:12 PM | |
Posts: 9 Rating: (0) |
They both pulse. |
9/15/2014 9:18 PM | |
Joined: 2/8/2012 Last visit: 12/22/2014 Posts: 2347 Rating: (385) |
Then this should work ... |
This contribution was helpful to2 thankful Users |
9/15/2014 9:48 PM | |
Posts: 9 Rating: (0) |
It did! Thank you very much!
|
Follow us on