6/6/2011 12:35 AM | |
Joined: 7/2/2008 Last visit: 4/5/2024 Posts: 928 Rating: (305) |
Dear All, A small thing to clarify, It's not limited only to fail safe (expensive) modules but the following standard modules could alsobe used for 1ms time stamping. 6ES7321-7BH01-0AB0. 6ES7321-7RD00-0AB0. 6ES7321-7TH00-0AB0. 6ES7326-1BK01-0AB0. It could also be configured with ET200iSP (6ES7131-7RF00-0AB0) More information can be read under System and componentsin High-Precision Time Stamping (V7.1). Another application I know is the power distribution. It's used in substations to clarify which circuit breaker has tripped first and what happened consequently. Best regards. H-H |
4/20/2012 2:53 PM | |
Joined: 3/18/2008 Last visit: 12/8/2023 Posts: 1750 Rating: (270) |
Dear All, Please find attached Scrrenshot for ready reference. Please note you can not check Alamsgenerated via MSG_TS Blockwithout Actual Hardware.i mean Checking of this High Precesiion TimeStamping Alarms are not possibleon PLC Simulator because Alarms are processed via ET200M Directlyto OS. AttachmentHigh Precision Time Stamping .zip (269 Downloads) |
VANDE MATARAM..... |
|
Follow us on