5/13/2020 12:42 PM | |
Joined: 3/14/2008 Last visit: 9/25/2024 Posts: 2097 Rating: (938)
|
Hi, The color cannot be changed since EMF files are created indicating a status. EMF files are created by Visio and you need the original visio files to modify them, which Siemens does not provide. You can create your own EMF files however. You can do this in WinCC Graphics Designer and export as EMF or by using PowerPoint or Visio and export the pictures as EMF+ format (Extended). You can then replace the EMF files under the Extended Status Display that shows the correct EMF for the correct status. A better way is to use the PCS7CustomPictures folder. As of PCS7 V8.1 the PCS7CustomPictures folder is automatically created in the GraCs folder when the OS project editor is opened. It is the default folder for custom pictures. You can configure the representation of custom pictures of APL block icons in the properties of the APL block icon: Configurations->"Folder for pictures" attribute As for the MonDiL, there are colors available which can be set as background color. This can be modified via the "Color" variable. See the help file of MonDiL under section: Adapting the color representation in the configured message class. If this is unwanted, I guess the only thing left is to modify the C-script in the faceplate. The colors that can be set are distributed to the OS by setting bits in Status3. For example: If the Color variable is set to value 6 (=Violet), bit 20 is set in Status3. A script is used to check the bit in the Status3 and then the correct color will be set. You can change this by setting a specific color yourself, but you will need knowledge of scripting in order to proceed with this.
|
Last edited by: Oreca at: 05/13/2020 13:18:26Last edited by: Oreca at: 05/14/2020 09:42:35Expanded text MonDiL with an example If I could help you, you can use the RATE button. Thank you. |
|
Follow us on