2/14/2012 2:11 PM | |
Joined: 10/26/2011 Last visit: 9/9/2024 Posts: 762 Rating: (191) |
How can I export all of the tags in Tag Logging to a CSV file? Does the system provide a way to export the tags configured, and the tags configured for Tag Logging, to a CSV file? Solution No, there is no standard way, however, the attached script will allow for exporting this information to a CSV file. Instructions are in the attached txt file. This was developed on PCS 7 V7.1 SP 1. AttachmentInstructions.zip (582 Downloads) |
Last edited by: Thunderstorm at: 3/2/2016 6:51:56 PMSIMATIC PCS 7 - Overview |
|
This contribution was helpful to1 thankful Users |
3/2/2016 12:45 PM | |
Posts: 43 Rating: (0) |
Hi Thunderstorm, can I apply into PCS 7 V8.0 Sp1. Is there any impact on it if not applicable? |
Follow us on