11/28/2018 8:13 PM | |
Joined: 4/9/2016 Last visit: 12/9/2018 Posts: 2 Rating: (0) |
The same problem I have with Excel 365. Item 2.3 of the manual. In Add-in tab there no LogoAccessTool menu appears. All the LOGOVAR functions in Excel are installed. Just the menu. Some ideas ...? On my tablet with Excel 2016 everything works fine. Tadeusz ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 11/29/2018 8:21:10 AMNew subject after splitting |
|
12/7/2018 3:18 PM | |
Joined: 9/19/2018 Last visit: 5/10/2024 Posts: 376 Rating: (46)
|
Hey tepe77, please note that LOGO! Access Tool only supports following excel versions (see attachments: - Office Excel 2007, 2010, 2013 (both 32-bit version, and 64-bit version) So this can lead to this behavior with Excel 365. Yours LOGO! Support! LOGO! Access Manual: |
12/9/2018 6:43 PM | |
Joined: 4/9/2016 Last visit: 12/9/2018 Posts: 2 Rating: (0) |
Hi Thanks for the answer. Fortunately LogoAccessTool works well on Yoga tablet with Office 2016 32 bit. Regards |
4/27/2020 4:09 PM | |
Posts: 1 Rating: (0) |
Is this going to be fixed soon? My entire company have moved to Office 365 and i now cant use the tool. |
Follow us on