2/27/2020 10:48 PM | |
Joined: 3/14/2008 Last visit: 9/17/2024 Posts: 2095 Rating: (936)
|
Hi voyager1963, I checked the Compatibility Tool for you and the compatibility lists, but I cannot find any reference regarding Windows Server 2016 Long-Term Servicing Channel. The only version that is compatible with PCS7 V9.0 SP1 + Cemat V9.0 Upd1/SP1 is: - Windows Server 2016 x64 Standard edition - Windows Domain Controller 2016 x64 Standard - Windows Domain Controller 2016 Datacenter edition x64. Note: When using the Domain Controller, please bear mark: Operating system information on PCS 7 V9.0 SP1
Maybe if you check the following topic: Link, you may find a solution for your problem, but I have to say this....please use only the released Windows version for your Process Control System. |
Last edited by: Oreca at: 02/27/2020 22:56:01If I could help you, you can use the RATE button. Thank you. |
|
6/1/2021 7:46 AM | |
Joined: 5/6/2020 Last visit: 8/13/2024 Posts: 32 Rating: (1) |
Hi Are you sure that Cemat V9.0 SP1 is compatible with Windows server 2016 Standard? I just tried it and could not install it. It shows the message that it can not be installed on Server 2016. Can you help me on the version of PCS7 and Cemat that can be installed on Server 2016? |
Follow us on