5/13/2016 9:13 AM | |
Joined: 9/16/2013 Last visit: 3/12/2024 Posts: 199 Rating: (23) |
This is the third thread with the same question. https://support.industry.siemens.com/tf/de/en/posts/148004/ https://support.industry.siemens.com/tf/de/en/posts/69609/ Surprise: The same anser, you can directly read and write the Data of the telegrams. here with safety and here without you will find a lots of Information, how a g120 and normal step7 cpu (non PCS7) can work together |
Last edited by: Gordon Shumway at: 5/13/2016 9:14:39 AMadded link without safety |
|
5/13/2016 9:22 AM | |
Joined: 5/26/2011 Last visit: 1/10/2024 Posts: 455 Rating: (7) |
Hello sir Gordon, Sorry if it's seems like a duplicate post but as I understood it's a bit different question now. I thought what sir Mark said is that we need libraries for Telegram 20 and Telegram 352 and that you said that we can integrate without libraries only on Standard Telegram 1 (only 2 input/output WORD). Now I found that we need at least Telegram 20 (for current and torque values). So my question now is maybe we can also do integrate without libraries on Telegrams 20 (or maybe also Telegram 352?), after I also found that we are actually selecting what telegram to use on HWconfig GSD? So I take it that you answered positive also for Telegram 20? |
Last edited by: G_R_E_Y at: 5/13/2016 9:24:54 AMLast edited by: G_R_E_Y at: 5/13/2016 9:27:14 AMLast edited by: G_R_E_Y at: 5/13/2016 11:37:08 AM |
|
5/13/2016 9:27 AM | |
Joined: 9/16/2013 Last visit: 3/12/2024 Posts: 199 Rating: (23) |
you can directly read and write the Data of the telegrams. The telegram number only tells how Long the telegram is and which data is connected at sinamics side per Default G120 operating instructions. This document will have an answer to almost every question which is g120 related |
Last edited by: Gordon Shumway at: 5/13/2016 9:34:16 AM |
|
5/13/2016 9:46 AM | |
Joined: 5/26/2011 Last visit: 1/10/2024 Posts: 455 Rating: (7) |
Thanks for this answer (and I'm sorry I didn't get this on the previous post)! |
Follow us on