7/22/2019 6:10 PM | |
Joined: 4/2/2009 Last visit: 3/25/2024 Posts: 5 Rating: (1) |
Hi, I'm looking at this same application with nickcat65 and what we are trying to do is use 2 x AI for temperature inputs and an adjustable setpoint which we would like to adjust using the TDE. If we wanted to use VW0 as an example, which we have in a simple project to test, as the setpoint, there doesn't appear to be any way of getting this VW0 as an Input/Output variable on the TDE as the only data that is avaliable is the Bxxx Blocks when editing the message block. In the simulation we use the datatable to adjust the value. Is there any way of inputting data into VW0 via a TDE ?? Many Thanks ------------------------------------------------------------------------------------------ |
Last edited by: DATEK at: 07/22/2019 18:13:17Last edited by: Jen_Moderator at: 07/23/2019 06:38:09New subject after splitting |
|
Follow us on