5/25/2019 11:15 AM | |
Joined: 2/22/2008 Last visit: 8/6/2024 Posts: 2698 Rating: (207) |
I don't know, if it is possible to communicate without a program. I think so that it's enough. With a little test program you are able to look for different functions of Modbus, see attached test program. There are comments for the right registers and the function codes you can see in my table. If have activated 2 servers, Modbus and S7. You can delete one of them, but it doesn't matter for testing with both servers. Regards, Scorp AttachmentTest.zip (222 Downloads) |
Follow us on