9/11/2020 4:13 PM | |
Joined: 11/15/2019 Last visit: 9/19/2024 Posts: 63 Rating: (0) |
Yes, you're right. 0-100% includes only the speed of the pump (hz). which can vary. |
9/12/2020 7:47 AM | |
Joined: 12/18/2014 Last visit: 9/23/2024 Posts: 33816 Rating: (4201)
|
A small example in the attachment. You only have to change the IP addresses in the LOGO! program and in the TIA project (under connection) to your IP addresses. AttachmentRobijn.zip (290 Downloads) |
9/14/2020 5:21 AM | |
Posts: 2 Rating: (0) |
Danfoss MCA122 is a modbus tcp card. |
This contribution was helpful to1 thankful Users |
11/25/2020 5:08 PM | |
Joined: 12/18/2014 Last visit: 9/23/2024 Posts: 33816 Rating: (4201)
|
In attachment both variants.
AttachmentRobijn.zip (203 Downloads) |
Follow us on