5/17/2010 1:52 AM | |
Joined: 3/26/2009 Last visit: 2/3/2022 Posts: 43 Rating: (11) |
ok here it is sorry Fred AttachmentLogodataLogger2010a.zip (1178 Downloads) |
This contribution was helpful to10 thankful Users |
5/19/2010 3:52 PM | |
Joined: 3/26/2009 Last visit: 2/3/2022 Posts: 43 Rating: (11) |
Just a little info you can not run the logo software and the logger at the same time. Fred |
6/2/2010 11:13 PM | |
Joined: 3/26/2009 Last visit: 2/3/2022 Posts: 43 Rating: (11) |
i will look into this and get back to you by the weekend. Fred |
6/5/2010 4:50 AM | |
Joined: 3/26/2009 Last visit: 2/3/2022 Posts: 43 Rating: (11) |
PETER, I fixed the issue with the flags and it now works.see the revised logger. fred AttachmentLogodataLogger2010aREVISED.zip (751 Downloads) |
This contribution was helpful to1 thankful Users |
6/5/2010 9:42 PM | |
Joined: 3/26/2009 Last visit: 2/3/2022 Posts: 43 Rating: (11) |
Good afternoon everyone, I used the data logger on an analog project and the logger recorded the analog values. I was using percentage.I will experiment with temperature next. Fred AttachmentLogodataLogger2010aANALOG.zip (696 Downloads) |
This contribution was helpful to1 thankful Users |
6/6/2010 12:41 AM | |
Joined: 3/26/2009 Last visit: 2/3/2022 Posts: 43 Rating: (11) |
Sorry for another change , i added a reset button to the logger.So now you can reset back to row 11 with one push of the button. Fred AttachmentLogodataLogger2010aANALOG.zip (735 Downloads) |
Last edited by: derf nedraw at: 6/6/2010 1:04 AMLast edited by: derf nedraw at: 6/6/2010 12:41 AM |
|
This contribution was helpful to2 thankful Users |
6/6/2010 11:19 AM | |
Posts: 21 Rating: (0) |
Hello again, and thanks for your work. Unfortunately I still can’t log my flags. I have attached my program so you can see what I’m looking for. In the bottom right corner there are two flags (M1 and M2) that indicate the status of my valve in this solar heating setup. One flag if the valve is open and one flag if the valve is closed. But in the file both M01 and M02 shows “0” at all times. Am I looking at the wrong ID? AttachmentPool_controler.zip (786 Downloads) |
6/7/2010 1:14 AM | |
Joined: 3/26/2009 Last visit: 2/3/2022 Posts: 43 Rating: (11) |
Drogen, Try this logger this one works. fred AttachmentLogodataLogger2010a verson 2.zip (449 Downloads) |
This contribution was helpful to1 thankful Users |
6/8/2010 9:33 PM | |
Joined: 3/26/2009 Last visit: 2/3/2022 Posts: 43 Rating: (11) |
Hello everyone, I have updated the data logger, it now can log the date with the time, do analog, and flags, clear the content of the cells and reset start to cell 11.I can think of anything else i can do for the logger. I hope everyone finds it useful. Fred AttachmentLogodataLogger2010a verson 2 .zip (425 Downloads) |
This contribution was helpful to2 thankful Users |
6/9/2010 5:50 AM | |
Posts: 21 Rating: (0) |
Thanks, thats great. I have been missing the "date-thing" but done it manually in Excel. Now it has what i need. |
6/24/2010 4:08 PM | |
Joined: 3/26/2009 Last visit: 2/3/2022 Posts: 43 Rating: (11) |
Hello , I noticed a lot of downloads on the original data looger file The file that is attached to this message is the latest and greatest. I weanted to make sure that everyone using the data logger has the correct one. Fred (derf) AttachmentLogodataLogger2010a verson 2 .zip (694 Downloads) |
6/24/2010 7:14 PM | |
Joined: 3/26/2009 Last visit: 2/3/2022 Posts: 43 Rating: (11) |
chyde, that is what the forum is all about , helping others. Fred (derf) |
6/24/2010 8:25 PM | |
Joined: 5/9/2010 Last visit: 4/1/2024 Posts: 50 Rating: (7) |
well done, thanks a lot for this great logger |
This contribution was helpful to1 thankful Users |
6/24/2010 8:30 PM | |
Joined: 3/26/2009 Last visit: 2/3/2022 Posts: 43 Rating: (11) |
bobbt, thanks Fred (derf) |
Follow us on