2/21/2020 2:31 PM | |
Joined: 12/18/2014 Last visit: 4/18/2024 Posts: 32843 Rating: (4061)
|
Hello BoCari, at first welcome to the forum.
Here is just a user forum. If you want statements from Siemens, you have to start a Support Request. To 1.) I don't work much with LAD, so I can't say anything about possible errors when converting to FBD. To 2.) The current demo version is V8.0. The current version of the licensed software is V8.2.1.
|
This contribution was helpful to1 thankful Users |
2/21/2020 3:40 PM | |
Posts: 8 Rating: (0) |
AttachmentSFC - 1.zip (111 Downloads) |
2/21/2020 3:52 PM | |
Joined: 12/18/2014 Last visit: 4/18/2024 Posts: 32843 Rating: (4061)
|
This is an old bug in the LSC V8.0 software. Errors occurred when the connections between the blocks were broken. I loaded the program with the current version V8.2.1 and converted it to LAD. Everything is fine there. AttachmentLOGO!Soft Comfort - SFC - 3.pdf (119 Downloads) |
This contribution was helpful to1 thankful Users |
2/21/2020 3:55 PM | |
Posts: 8 Rating: (0) |
HI Scorp, Program is in FBD designed; also attached. Once converted into LAD, it doesn't give the same endresults when running in simulation. AttachmentSFC - 1.zip (82 Downloads) |
2/21/2020 4:08 PM | |
Joined: 12/18/2014 Last visit: 4/18/2024 Posts: 32843 Rating: (4061)
|
Here the converted program. Converted from FBD to LAD by using LSC V8.2.1. AttachmentSFC - 2 (Converted from FBD to LAD by V8.2.1).zip (109 Downloads) |
This contribution was helpful to1 thankful Users |
2/21/2020 6:05 PM | |
Joined: 12/18/2014 Last visit: 4/18/2024 Posts: 32843 Rating: (4061)
|
With fullversion of LSC V8.0 is the error also.... |
Follow us on