4/4/2011 6:23 PM | |
Posts: 3 Rating: (0) |
hi.can some one read a protected logo program?is it possible? |
4/4/2011 6:35 PM | |
Joined: 3/21/2006 Last visit: 9/10/2024 Posts: 10228 Rating: (1181) |
Everything is possible. Just ask for password. Best regards, Hristo Mihalev |
5/9/2011 2:42 AM | |
Posts: 7 Rating: (0) |
You have to know the password to access the program. |
5/9/2011 11:05 AM | |
Posts: 154 Rating: (17)
|
without the password you only can delete the password including the program. So you can use the LOGO! again, but you have also to program the LOGO! again. Under the following link you can find a description to delete program and password: delete password |
This contribution was helpful to1 thankful Users |
5/23/2011 7:38 PM | |
Joined: 10/22/2008 Last visit: 9/19/2024 Posts: 369 Rating: (5) |
In elder Logo! it was possible to get/read password. Look in google. |
5/24/2011 10:07 PM | |
Joined: 12/27/2006 Last visit: 8/18/2024 Posts: 1197 Rating: (113) |
The general password fos all the LOGO!'s is * * * * |
5/24/2011 10:26 PM | |
Joined: 1/5/2007 Last visit: 4/7/2023 Posts: 1690 Rating: (580)
|
Hi, that is a joke, isn´t it? Best regards Betel |
==> Meine TAG-Listen: "deut." |
|
5/24/2011 10:28 PM | |
Posts: 8946 Rating: (999) |
Yes, that was a joke of course..... All passwords ever are **** :-) |
5/24/2011 10:31 PM | |
Joined: 12/27/2006 Last visit: 8/18/2024 Posts: 1197 Rating: (113) |
Even there are other passwords p.e * * * * * But al the LOGO! s use 4 stars |
5/25/2011 8:31 AM | |
Joined: 10/22/2008 Last visit: 9/19/2024 Posts: 369 Rating: (5) |
To make it easier to guess password it is only possible to use charakters (A-Z). |
Follow us on