1/16/2020 4:45 PM | |
Joined: 2/22/2008 Last visit: 8/6/2024 Posts: 2698 Rating: (207) |
I don't think so, that all values are changed with one entry at the right point. See also the Link in german conference, last post at 18.11.2019. There is also a PDF file with german comments inside. Regards, Scorp |
1/18/2020 9:13 AM | |
Joined: 2/22/2008 Last visit: 8/6/2024 Posts: 2698 Rating: (207) |
Up to know i never have used custom web pages at home or in our company, therefore i have only searched for an easy way to manipulate some actual values, e.g. temperature display 23.5°C. This only should be the help for other people in the conference. If someone is fit with HTML5 programming, he can do much more. See Link for more information of LWE. In chapter 4 is a description of the HTML development interface including a callback function to update editable values. Regards, Scorp |
1/18/2020 4:01 PM | |
Joined: 12/17/2012 Last visit: 10/2/2023 Posts: 9 Rating: (0) |
I attach an example with two variables, 1stand 2nd. When I modify only the 1stvariable from main.htm there is no decimal shown. When I modify only the 2nd variable there appears to be a decimal to both variables. Is it reasonable? (the modification is var actVal = (value / 10).toFixed(1);) Attachmentexample.zip (87 Downloads) |
Follow us on