12/12/2011 10:24 AM | |
Joined: 10/26/2011 Last visit: 9/9/2024 Posts: 762 Rating: (191) |
Hello DannM Which operations system has the Microbox 427C? I think, it is a Windows embedded system. If this is a windows embedded system, than you cannot install an OS Server. The 627 B is an older one. Which PCS 7 version to you want to use? PCS 7 version 7 SPx? |
SIMATIC PCS 7 - Overview |
|
12/12/2011 1:50 PM | |
Joined: 10/26/2011 Last visit: 9/9/2024 Posts: 762 Rating: (191) |
Hello You cannot have a single station (ES / OS) ona mBOX. You have to use the Box PC. You have Server 2003 on the Box PC, and I think, that there is only WinCC installed. You cannot install the Engineering Package over this installation (it is not running, I don't know why. I treid this in the past). You have to do a new installation of the Box PC with Windows XP or Server 2003 and after that PCS 7. At the moment, I don't know, if it is allowed to use a WinLC on a Single Station! I will look for... Regards |
SIMATIC PCS 7 - Overview |
|
12/12/2011 1:58 PM | |
Joined: 10/26/2011 Last visit: 9/9/2024 Posts: 762 Rating: (191) |
... me again. To the WinLC / RTX. You can buy a bundle box PC with ES / OS / AS. BUT you cannot buy only the License RTX (SIMATIC PCS 7 V7.1 Runtime License RTX). It is impossible to get only this license! Regards |
SIMATIC PCS 7 - Overview |
|
12/12/2011 3:03 PM | |
Joined: 5/22/2011 Last visit: 8/1/2024 Posts: 17 Rating: (1) |
mmm... In my case I can use licence from microbox PCS7 AS RTX. I think I must upgrade OS to SP3.. |
12/12/2011 5:34 PM | |
Joined: 10/26/2011 Last visit: 9/9/2024 Posts: 762 Rating: (191) |
It is recomment tohave the neweset updateofWindows. |
SIMATIC PCS 7 - Overview |
|
12/12/2011 11:34 PM | |
Joined: 5/22/2011 Last visit: 8/1/2024 Posts: 17 Rating: (1) |
I hope that 'll be work. Thanx Dann. . |
Last edited by: DannM at: 12/12/2011 11:34 PM |
|
Follow us on