2/15/2017 8:49 PM | |
Joined: 1/24/2009 Last visit: 3/29/2024 Posts: 85 Rating: (7) |
Hello, it is the 1st time that i need to establish a MODBUS communication between S71200 CPU1217 using CM1241 RS422/485 module and a NETWORK Analyzer instrument in order to read in my plc code values of voltage, current etc. I have prepared PLC as Master and the Analyzer as slave. Analyzer has no choice for MAster - Slave in it's confuguration menu but we will see... A critical problem is that it is not possible to make a real simulation in my office because the Analyzer is already installed at the plant. The scope is : using PLC as Master i need to to read contunuously 85 Dwords from the Slave = Analyzer with adress 31. There is no need to write to the slave anything, just to read. Attached the 3 networks where i have prepared the plc code in TIA Portal. 1. Is it necessary to declare adress to Master ? or need to declare somewhere that plc is the Master ? 2. I need after the end of a data transfer, to start a new request. Is my plc code ready to do that ? 3. Is it able to read all the 85 Dwords with each request or must i do a trick ? According to TIA help only 122 words per query is allowable to read. 4. In DATA_PTR udt i have declared the 85 Dwords that i have to read continously from the Slave - Analyzer. 5. In Modbus_Master module at input DATA_ADDR must be always the 1st memory position of Modbus 40001. Also in input DATA_LEN must put the value 170 ? And finally in input MB_ADDR must put the slave's adress ( 31 ) ? Sorry for large explanation. I hope this topic to help others too ! AttachmentMODBUS_ConnX.pdf (609 Downloads) |
2/17/2017 12:22 PM | |
Joined: 1/24/2009 Last visit: 3/29/2024 Posts: 85 Rating: (7) |
Hello again dear ola84, attached my code to read from slave 85 Dwords ( in 2 steps because of reading limit of 122 words ) Step 1 : reads the first 80 words ( 40 Dwords ) Step 2 : reads the rest 90 words ( 180 Dwords ). I kindly ask your time, to check it if everything works ok and if possible to suggest me a more efficient way to handle this communication. Do you see any erros in that code ? AttachmentModbus1.pdf (495 Downloads) |
2/17/2017 2:04 PM | |
Joined: 2/22/2016 Last visit: 8/28/2022 Posts: 140 Rating: (30) |
Hi Kosmous. If it's critical that you software works when you go to the plant, then I suggest you use another plc to simulate a modbus slave. AttachmentModbus1.pdf (479 Downloads) |
Please use the contact form in the link below if you will like to come in contact with me. I don't check personal messages frequently. |
|
This contribution was helpful to1 thankful Users |
2/17/2017 3:04 PM | |
Joined: 1/24/2009 Last visit: 3/29/2024 Posts: 85 Rating: (7) |
Your suggestion are right . In your comments Reset of REQ is making when DONE is true may be ? |
2/17/2017 4:13 PM | |
Joined: 2/22/2016 Last visit: 8/28/2022 Posts: 140 Rating: (30) |
There are many ways to Rome ! :) I am not sure if that will work or not, but I do know it will work if you set REQ false right away after the MB_MASTER block. I am worried that a new request will start before the new query parameters has been inserted. But I am not sure about this. If you have a rs-232/rs-485 converter, you can connect a PC to the modbus line and "lisen" to the telegram with a modbus software. One other thing you should be award of, is the endianness of your revived data. Modbus is easy and light protocol, but there are a lot of pitfalls ! |
Please use the contact form in the link below if you will like to come in contact with me. I don't check personal messages frequently. |
|
2/17/2017 4:52 PM | |
Joined: 1/24/2009 Last visit: 3/29/2024 Posts: 85 Rating: (7) |
thank you for your time, i will check it in real time during commisioning and come back to update the forum. |
3/1/2017 6:57 PM | |
Joined: 1/24/2009 Last visit: 3/29/2024 Posts: 85 Rating: (7) |
Dear ola84, after checking on site, reading process works on a right way but only when running only step1 ( until Network 4 ) There is a limit from the slave side, of 48 words for reading during each REQuest. I have tottaly to read 170 Words, so i must read 170 Words in 4 steps. When step2 is running ( Network 5 and 6 ), "done" bit is triggered but error 8200 occurs random. It seems that a new REQuest is on, but in the same time, the previous request has not been completed yet. Do you think a time delay in Network 5 is the right solution ? 2. Step 1 ( until network 4 ) works only if start adress is 40002 and not 40001. Attached the code in order to help somebody else, maybe for reading at once and not in multiple steps AttachmentModbus2.pdf (264 Downloads) |
Last edited by: kosmous at: 3/3/2017 7:39:16 AM |
|
3/1/2017 9:17 PM | |
Posts: 3093 Rating: (322)
|
Hello Kosmous, Regards, |
3/2/2017 10:38 AM | |
Posts: 3093 Rating: (322)
|
No, as long as you evaluate the outputs of MB_MASTER correctly, no time delay is required. |
3/3/2017 10:24 AM | |
Joined: 1/24/2009 Last visit: 3/29/2024 Posts: 85 Rating: (7) |
Could somebody check the attached code in order to suggest the best solution for the above problem ? AttachmentModbus2.pdf (254 Downloads) |
Last edited by: kosmous at: 3/3/2017 10:24:57 AM |
|
3/3/2017 4:15 PM | |
Joined: 1/24/2009 Last visit: 3/29/2024 Posts: 85 Rating: (7) |
Hello ola84, thank you for your interest, you ere right, but i already use the RESET to REQ immediately after Master call. ( See attached ) Just it was not appeared in the pdf file that i had attached. The problem still remains. The communication is established, leds are blinking, the slave responds that communication is ok, but every 2 sec, error 8200 is appeared for 1 sec and dissapered again cyclically. When i use "done" contact in Network 6 in series with " busy normal close ", 8200 error is never appeared, but do i lose data in that way ? When only step 1 is called, everyhting works perfect ! May be i need to check somewhere the "done" bit before start step 2 ? AttachmentModbus_3.docx (249 Downloads) |
Last edited by: kosmous at: 3/3/2017 4:25:18 PMLast edited by: kosmous at: 3/3/2017 4:43:14 PMLast edited by: kosmous at: 3/3/2017 4:43:31 PM |
|
3/4/2017 10:23 AM | |
Joined: 1/24/2009 Last visit: 3/29/2024 Posts: 85 Rating: (7) |
Hello ola84, many thanks for your suggestion. You are right ! The only strange issue now is that when start adress to read the slave is 40001, error 8383 still occurs even if i try to read only 2 words. Error 8383 means : " Error in the data address or address outside the valid range of DATA_PTR " When starting adress for reading process is 40002, no error occurs ! Attached is the structure of the adress that slave demands. Do you see anything strange issue about 1st reading register 40001 ? ------------------------------------------------------------------------------------------------- By the way, to help somebody else, my communication process worked with MODBUS blocks of TIA PORTAL and not with MODBUS ( RTU ) blocks. AttachmentPLC reads form this slave device.pdf (358 Downloads) |
Follow us on